All Posts
Written by Tim Staelens
The torque-to-capacity relationship for helical anchors and piles is an empirical method originally...
Written by Ryan Freeman
With the recent and upcoming revisions of IEEE C62.11 and IEC 60099-4 surge arrester standards,...
Written by Mike Kryman
Not sure what the proper bushing replacements are for your in-service bushings? Hubbell | PCORE®...
Written by Joseph Cardona
Insulating rubber blankets for energized line maintenance come in a variety of sizes, classes and...
Written by Tim Staelens
Predicting the holding capacity of an anchor can be difficult due to soil variations at different...
Written by Tim Staelens
The reliability of our overhead power and communication lines is as important today as ever before....
Written by Mike Kryman
Repairing a bushing is less expensive than purchasing a new bushing and you are able to maintain...
Written by Haley Engel
Utilities recognize that wooden poles are vulnerable to fire. However, replacing millions of wooden...
Written by Tamera Weedon
A common cause of power quality issues in underground systems is the improper torquing of...
Written by Jeff Kopp
During this time of heightened concern for cleanliness, here are some guidelines for additional...
Written by Haley Engel
Polymer compounds suitable for electrical insulation can consist of 10 or more ingredients which...
Written by Haley Engel
After defining the characteristics required of an ideal polymer housing material, the next step is...
Written by Haley Engel
It’s a commonly held belief that the single most important characteristic for insulating materials...
Written by Billy Webber
Prior to 2009, ASTM F855, Standard Specifications for Temporary Protective Grounds to Be Used on...