HUBBELL POWER SYSTEMS
HUBBELL POWER SYSTEMS

Tips on Managing Arc Flashovers

Tips to manage an arc flashover created when an electrical discharge goes through air. It can cause a bright light and damage the two objects it lands on.

An arc flash or arc flashover occurs when an electrical discharge goes through air. It can cause a bright visible light as well as damage the two objects it lands on.

Arc Flashover.png

When a hotline tap clamp is installed directly on a main line the arc goes from the bill of the hotline tap clamp to the main line.

However, when a stirrup clamp is used, the arc goes from the bill of the hotline tap clamp to the bail of the stirrup, thus eliminating damage to the main line.

 

 

 
SUBSCRIBE TO NEWSLETTER