HUBBELL POWER SYSTEMS
HUBBELL POWER SYSTEMS

Installing Screw Displacement Piles

Screw displacement piles are provided in easy to handle lengths up to 20'-0 long and can be installed with a track-hoe excavator, typically less than 30,000 lbs machine. The torque is measured during installation to prevent damage to pile, and the pile advances and displaces soil at the same time.

Installing CHANCE® Drivecast™ Screw Displacement Piles

As the CHANCE® Drivecast™ screw displacement pile is rotated into the ground, it compresses the soil laterally, creating a void which is immediately filled with grout maintained in the reservoir. The schedule 80 centralized shaft replaces the rebar cage as column reinforcement. 

Grout is released from a gravity-fed reservoir located at the surface prior to the advancement of the lead section into the soil and is continued until the minimum column length is achieved. 

Grout is typically a 4500 psi mix, either neat or with a sand aggregate filler. It is placed into the reservoir immediately prior to the advancement of the lead section into the soil. The volume of grout contained in the reservoir is always maintained at a level to maintain positive hydrostatic pressure on the grout column. Grout placement continues until the Drivecast pile installation is completed. 

Installation ProcessInstalling CHANCE® Drivecast™ Screw Displacement Piles

  • CHANCE Drivecast screw displacement piles are provided in easy to handle lengths up to 20'-0 long
  • Installed with a track-hoe excavator - typically less than 30,000 lbs machine
  • Torque measured during installation to prevent damage to pile
  • Pile advances and displaces soil at the same time
  • Rate of penetration is approximately 3" per revolution
  • Rate of revolution: 5-15 RPM

Installation Equipment

A rotary type, hydraulic power driven torque motor should be utilized, along with a Kelly bar adapter and drive tool. The reservoir allows immediate knowledge of grout consumed if used as a graduated column.

GET THE CHANCE DRIVECAST PILE BROCHURE