HUBBELL POWER SYSTEMS
HUBBELL POWER SYSTEMS

How Automatic Transfer Switches Support Distribution Automation & Utility Reliability

Learn how distribution automation, automatic transfer switches, and SCADA integration improve reliability in underground distribution networks

How Automatic Transfer Switches Support Distribution Automation & Utility Reliability
9:59

Reliable power has become essential to modern life. Hospitals, data centers, telecommunications networks, and industrial facilities depend on continuous electrical service to maintain operations, making even brief outages costly and disruptive. As communities grow and infrastructure becomes increasingly connected, utilities face increasing pressure to improve reliability while minimizing service interruptions.

To meet these evolving reliability requirements, utilities are increasingly investing in distribution automation technologies that improve visibility, accelerate response times, and reduce outage durations.

One proven strategy is using an automatic transfer switch (ATS), which enables underground medium-voltage distribution networks to automatically transfer loads between power sources when system disturbances occur. In practical terms, an ATS helps utilities maintain service continuity by automatically switching customers to an alternate power source when disruptions occur.

By combining intelligent controls, system monitoring, and motor-operated switchgear, utilities can improve reliability, strengthen grid resiliency, and support the growing demands of critical infrastructure.

What is an Automatic Transfer Switch?

An ATS is a device that automatically transfers an electrical load from a primary power source to an alternate source when abnormal operating conditions are detected. These conditions may include:

    • Loss of voltage
    • Undervoltage events
    • Sustained overcurrent conditions
    • Feeder outages or source failures

Once the abnormal condition has cleared and the primary source is confirmed to be stable, the ATS automatically returns the load to the preferred power source.

The primary objective of automatic transfer switching is to maintain service continuity while minimizing disruption to customers. In underground medium-voltage distribution networks, automatic transfer switches help utilities provide near-continuous power to facilities where reliability is essential.

Why Automatic Transfer Switches Are Essential for Critical Infrastructure

Today's electrical grid serves a growing range of critical infrastructure that depends on uninterrupted power. As grid modernization expands and operational processes become increasingly automated, even momentary power interruptions can have significant consequences.

Common applications for automatic transfer switches include:

    • Hospitals and healthcare facilities
    • Large-scale data centers
    • Emergency response and public safety centers
    • Military and defense installations
    • Critical manufacturing operations
    • Telecommunications and network infrastructure

For these customers, reliability is more than a performance metric. It is an operational requirement. An ATS helps ensure these facilities continue receiving power by rapidly transitioning to an alternate source when disruptions occur.

As utility customers continue to demand higher levels of service reliability, automatic transfer switches are becoming a vital component of broader grid modernization and distribution automation initiatives.

How an ATS Works in Underground Medium-Voltage Distribution Networks

In underground medium-voltage distribution networks, ATS devices are commonly deployed using motor-operated switchgear integrated with sensing, communications, and control technologies.

Under normal operating conditions, the primary power source is connected to the distribution system and continuously monitored through current and voltage sensors. These measurements are transmitted to a remote terminal unit (RTU), which evaluates system conditions against predefined operating thresholds.

The RTU communicates with the utility's SCADA system, providing operators with real-time visibility into network performance, system status, and event history.

The goal is simple: detect the problem, transfer the load, and restore service as quickly as possible. When a disturbance occurs, an ATS sequence typically follows these steps:

    • The primary source experiences a fault or loss of voltage.
    • Sensors detect abnormal operating conditions.
    • The RTU processes the event and initiates a transfer command.
    • The motor operator automatically switches the load to an alternate feeder or backup power source.
    • The primary source continues to be monitored.
    • After stable operating conditions are restored, the RTU initiates a transfer back to the preferred source.

This automated process can be completed in seconds—or even fractions of a second depending on application requirements—dramatically reducing outage duration compared to manual switching methods.

 

Figure 1. One-Line Diagram for Motor-Operated Switchgear ATS Application

Diagram for Motor-Operated Switchgear ATS Application

 

Figure 2. Typical ATS Sequence for Underground Distribution Networks

HUS-MULTI-GR-EN-04547_figure2

 

The Role of an ATS in Distribution Automation Strategies

Many utilities view automatic transfer switches as critical building blocks within larger fault location isolation and service restoration (FLISR) programs.

Distribution automation strategies are designed to quickly identify faulted areas, isolate affected sections of the network, and restore service to as many customers as possible. An ATS contributes to these goals by automatically transitioning loads to alternative power sources when outages occur.

When integrated with SCADA systems, RTUs, and automated switchgear, an ATS enables utilities to:

  • Improve outage response times
  • Reduce customer interruption durations
  • Enhance system visibility
  • Support self-healing grid initiatives
  • Improve reliability metrics such as SAIDI and SAIFI

As utilities continue modernizing underground systems, automatic transfer switches and distribution automation technologies are increasingly deployed together to create more resilient and responsive electric networks.

Key Benefits of Automatic Transfer Switches

Utilities deploy these automated switches to achieve several operational benefits:

  1. 1. Reduced Downtime: Traditional switching operations often require utility personnel to travel to the affected location and manually operate equipment. Using an ATS eliminates much of this delay by initiating source transfers immediately when abnormal conditions are detected.

  2. 2. Improved Reliability and Grid Resiliency: Automatic source transfer switching helps maintain service continuity by rapidly connecting customers to an alternate power source. This capability improves overall utility reliability and strengthens grid resiliency during outage events.

  3. 3. Faster Fault Detection and Response: Integrated sensors, RTUs, and SCADA-enabled distribution automation systems provide real-time visibility into system conditions. Automated responses allow utilities to identify and react to abnormal events significantly faster than manual processes.

  4. 4. Lower Operational Costs: Reducing truck rolls and manual switching operations can decrease long-term operating expenses while allowing personnel to focus on maintenance, restoration, and system improvement activities.

  5. 5. Enhanced Worker Safety: Automated switching reduces the need for personnel to perform manual switching operations in the field, limiting exposure to energized equipment and potentially hazardous conditions.

While automatic transfer switches depend on intelligent controls and communications, the switching equipment itself plays a critical role in successful operation. Utilities therefore need switchgear that can execute transfer commands reliably while integrating with broader automation systems.

How Motor-Operated Switchgear Supports Distribution Automation and Automatic Transfer Switching

As utilities expand distribution automation programs, motor-operated switchgear plays a central role in enabling automated grid operations.

Modern underground distribution systems require equipment that can respond quickly to system events while integrating seamlessly with utility communication and control platforms. Motor-operated switchgear provides the automation foundation necessary to support ATS applications and broader grid modernization efforts.

Solutions such as motor-operated air-insulated switchgear (AIS) enable utilities to automate source transfers, improve switching response times, and enhance visibility across underground medium-voltage distribution networks.

When combined with RTUs, sensors, and SCADA platforms, motor-operated AIS can help utilities create a smarter, more resilient network capable of responding automatically to changing system conditions.

Looking Ahead: Building a More Resilient Underground Distribution System

The demand for uninterrupted power will continue to increase as critical infrastructure expands, data consumption grows, and electrification accelerates across industries. Utilities are under increasing pressure to improve reliability while managing costs and maintaining safe operations.

Using an ATS in underground medium-voltage distribution networks provides a practical and proven approach to meeting these challenges. By leveraging distribution automation technologies such as motor-operated switchgear, SCADA integration, RTUs, and advanced monitoring systems, utilities can reduce outage durations, improve reliability, and strengthen overall system resiliency.

As utilities continue investing in grid modernization and distribution automation, automatic transfer switches will remain an important tool for improving reliability, reducing outage impacts, and supporting the evolving needs of critical infrastructure. 

Contact our utility experts to learn more about how automatic transfer switching solutions can support a more resilient grid.
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
Capacitor Banks for Volt-VAR Optimization

How Utilities Use Capacitor Banks for Volt-VAR Optimization

Continue Reading