Built to Last: Proven Longevity & Corrosion Resistance of Steel Foundations

Learn how hot-dip galvanizing, soil conditions, and field inspections support the long-term durability of Chance® Instant Foundations.

When specifying a foundation system, one of the most common questions engineers, utilities, contractors, and owners ask is: "How long will it last?"

For steel foundations, the answer often centers around corrosion resistance and long-term performance in real-world soil conditions. Fortunately, Chance® Instant Foundations are backed by decades of field experience and documented installations that demonstrate exceptional durability.

Why hot-dip galvanizing matters

Evaluations of foundations installed in the early 1980s reveal that hot-dip galvanized Chance Instant Foundations continue to provide reliable structural performance after more than four decades in service.

hot dip galvanizedChance Instant Foundations utilize hot-dip galvanized steel components manufactured to ASTM galvanizing standards. Typical zinc coating thicknesses range from approximately 4 to 7 mils, providing sacrificial protection to the underlying steel.

Unlike paint coatings that can be damaged or peel over time, galvanized zinc acts as a sacrificial anode that protects steel by corroding first. This sacrificial action helps preserve the structural steel beneath and significantly extends service life in a wide range of soil conditions.

Galvanized coatings provide:

    • Sacrificial corrosion protection
    • Long-term durability in soil environments
    • Low maintenance requirements
    • Proven performance over decades of field exposure
👉 Learn  about longevity: 50 Years of Instant Foundations

How soil conditions affect corrosion potential

Not all soils are equally corrosive. Two key indicators help predict the corrosion potential of buried steel foundations:

PleasantVal-1First, soil resistivity is used to evaluate corrosion potential. Lower resistivity indicates greater corrosion risk, while higher resistivity generally indicates lower corrosion potential.

Second, soil pH helps predict foundation longevity. Soils with a neutral pH near 7 are generally less corrosive than acidic soils with pH values near 5 or below.

According to Chance engineering guidance, well-draining soils with resistivity levels above approximately 2,000 ohm-cm can typically support a service life exceeding 50 years. That estimate does not mean the galvanizing is fully consumed after 50 years; rather, it indicates that expected material loss is generally not enough to compromise structural performance.

Field evidence from a decades-old installation

One of the most compelling examples comes from a Chance Instant Foundation installed in December 1983 at the Gibson Substation in Centralia, Missouri.

The foundation remained in service for more than 32 years before being excavated and analyzed in March 2016. Researchers evaluated galvanizing thickness, examined corrosion patterns, and inspected the steel for material loss.

The installation site included:

    • Surface gravel
    • Brown clay soils
    • Grey clay at helix depth
    • Poor drainage conditions
    • Saturated soil inside portions of the foundation during excavation

These conditions represent a demanding environment for any buried steel foundation.

After more than three decades underground, inspectors found:

    • Galvanizing still present on the foundation

    • Minimal corrosion on the upper and middle shaft sections

    • No significant steel loss affecting performance

    • Corrosion concentrated primarily near the lower shaft, helix, and base plate regions

    • Continued structural integrity of the foundation system

Researchers noted that discoloration visible on portions of the excavated foundation was not rust; when scratched, galvanizing remained present beneath the surface layer.

Chance Instant Foundation Report  - Signature GLS_Page_3Download the Corrosion Report


 

Historical galvanizing thicknesses for the foundation were estimated between 5 and 7 mils. Upon removal and inspection, measurable zinc remained across the foundation after more than three decades in service.

Using the most conservative measurements, engineers calculated a zinc loss rate of approximately 0.19 mils per year.

This result indicates exceptionally slow corrosion progression, even under relatively challenging soil conditions. At that rate, galvanized protection continues to provide decades of service before the underlying steel becomes exposed.

The Centralia corrosion study is not an isolated example of long-term performance.

Chance documentation also references transmission line foundations installed in Minnesota’s Tamarack Swamp in 1977, providing another long-term field example in a challenging soil environment.

The following photos show Chance foundations in Centralia, Missouri, that are still in use today. Based on the best available information, they were originally installed in the late 1960s, meaning they have been in service for more than 50 years. Zinc remains visible on the base plate, reinforcing the long-term durability demonstrated by these field installations.

 

Reliability and Service Life of CHANCE Helcial Piles1 Reliability and Service Life of CHANCE Helcial Piles 

These installations provide real-world confirmation that galvanized Chance foundation systems can deliver reliable performance over multiple generations of infrastructure.

What this means for specification decisions

As with any foundation system, expected service life should be evaluated using project-specific soil data, environmental exposure, loading requirements, and applicable engineering guidance. When evaluating foundation alternatives, life-cycle performance is every bit as important as initial installation cost.

The combination of:

    • Hot-dip galvanizing
    • Proven corrosion resistance
    • Documented field performance
    • Decades of successful installations
    • Predictable service-life modeling

gives engineers confidence that Chance Instant Foundations can provide dependable long-term support for lighting, utility, telecommunications, signage, and other infrastructure applications.

 



Recommended Posts

Pipe shaft helical pile being installed on lake shore

Helical Piles Support Custom Boathouse on Challenging Texas Shoreline

Continue Reading

Why Builders Are Turning to Helical Piles for Residential Construction

Continue Reading

Behavior of Square-Round Shaft Combination Helical Piles and Anchors

Continue Reading