- CHANCE® Foundation Solutions Blog
- Load testing
Load testing
Written by Dr. Alan J. Lutenegger, P.E., F. ASCE
One of the advantages often given for using helical anchors or piles is that they can be used...
Written by Mitch Westhues
Deep foundation and anchor testing according to ASTM D1143 and ASTM D3689 can be a cumbersome task...
Written by Ben Jennings, P.E.
Performing a load test is the best way to confirm pile capacity. It confirms if the pile has the...
Written by Ben Jennings, P.E.
Load testing is the only method that directly confirms pile performance under real soil conditions...
Written by Shawn Downey
As you will read, the compression test set-up posed several challenges that could be prevented with...
Written by Ian Romain, P.E.
Helical pile load testing is a field verification method used to confirm the axial capacity and...