Welcome the New Year with New Lighting

Progress Lighting offers a sneak peek of 300 new lighting fixture designs in January 2021.

January is almost here, and with it comes cold weather and New Year's resolutions. So why not make one of your resolutions to warm your home with the cozy glow of new lighting fixtures this year? It just so happens that January is also the time of year that Progress Lighting debuts brand-new lighting designs. With more than 300 new fixtures across eleven design lifestyles, we're sure to have lighting that complements your decor preferences. Here are some of the highlights from the winter lighting fixture debut.

Industrial styling meets luxe inspiration, creating fixtures that capture authenticity in detail yet offer a refined silhouette. For example, the Lorin pendant is elegantly designed, with sleek metal wires gathered by a smooth, wide metal collar, creating a stylized trumpet silhouette.

Suspended chandelier and pendant designs that appear to float effortlessly are paired with bold architectural forms and dangling artistic elements, inspiring endless design opportunities. The Parkhurst collection combines graceful curves and bold angles to create a softly structured look.

The Chilton exterior collection features a frosted glass cylinder suspended inside an open frame. Although its lantern styling is traditional in silhouette, the frame's spare, linear construction creates a modern impression.

Materials and finishes continue to be key themes in lighting designs. Soft gold tones, clean matte black finish and sleek satin white coatings are blended with textural frames, clear and white opal glass shades and linen-textured fabrics.

The Radian LED pendant has a domed metal shade supported by a contrasting cap and an interior finish that casts a warm glow of light.

The graceful silhouette of the Saffert pendant comes from four slender rods that capture a circular metal frame and glass diffuser. A fabric shade softens the clean style of the pendant.

A sleek update of Progress Lighting's perennially popular Air Pro Ceiling Fan leads the ceiling fan category, along with new fan designs that feature modern, industrial and coastal influences and WIFI technology.

In the functional lighting category, Progress has expanded its recessed lighting category with a complete line of LED options suitable for lighting needs in every room of the home. The integrated LED fixtures feature clean, modern silhouettes, high lumen output and integrated, color selectable CCT.

Inaugural Jeffrey Alan Marks Point Dume™
Exterior Lighting Collection.
This collection brings beauty and functionality to exterior living spaces. See a preview of the entire Jeffrey Alan Marks exterior collection here.

The new Progress Lighting introductions will be available at lighting showrooms, online retailers, and the Progress Lighting website, www.progresslighting.com.



Recommended Posts

Illuminate Your Space with LED Ceiling Fans

Illuminate Your Space with LED Ceiling Fans

Continue Reading
Designing with Light: Master 3 Trending Aesthetics

Designing with Light: Master 3 Trending Aesthetics

Continue Reading
New ways to light workspaces

New Ways to Light Workspaces

Continue Reading
Ï