Ceiling fans were initially introduced in the 19th century as mechanical devices designed to keep air circulating in a room, providing relief from oppressive heat. Their utilitarian nature prioritized function over form, with basic designs focused on efficiency rather than aesthetics. Today, ceiling fans are considered a design statement and an integral part of interior decor.
Our new collection of ceiling fans complements the interior design world's latest trends. From sleek and modern to vintage-inspired and eclectic, with intricately designed blades, unique finishes and integrated lighting elements, our new 2024 ceiling fans make a bold statement on a room's ceiling.
Trendsetting, Oscillating Fandeliers

Innovative in function and design, the new OSCILLAR™ Series of fandeliers features a compact silhouette with rings of integrated LED illumination and a trio of blades. A silent oscillating DC motor featuring a 360-degree rotation and six speeds delivers maximum air distribution in every direction throughout a room.
 |
Fanin Collection has a luxurious aesthetic from artisanal pressed glass and a beautiful metallic finish that reflects the light from integrated, dimmable edge-lit LEDs.
|
|
A dual-toned finish showcases the minimalistic design of the luxe industrial Burnett fandelier. State-of-the-art, dimmable LEDs cast up-and-down illumination ideal for indoor and covered outdoor settings.
|
 |
Our Shear fandelier is a masterpiece that elevates form and function to new heights. This gorgeous fan is crafted from swirling, beautifully finished metallic bands and creamy polished acrylic illuminated by innovative, linear, dimmable LEDs.
|
Fans Complementing the Latest Interior Design Trends

Modern organic design, luxurious aesthetics and clean contemporary styles are recurring themes that blur boundaries between function and form, with technologically advanced ceiling fans that contribute to the overall ambiance of a space.
-1.png?width=408&height=283&name=PROG_P250105-009-30_herolit_PRODIMAGE_1200%20(1)-1.png)
The Conte Indoor-Outdoor 56-inch LED Ceiling Fan is the epitome of modern sophistication and advanced technology, featuring a subtle, natural, organic design inspired by the delicate elegance of a blooming flower. A cutting-edge DC motor operates in serene silence while its integrated 20-watt LED light kit illuminates the space. Or conceal the light kit with the included coordinating blank plate if illumination is not desired.

Inspired by a delicate origami flower, the 60-inch Paso downrod ceiling fan features three sculpted ABS blades and a slim silhouette. Paso is UL dry location listed for indoor use, making it ideal for living rooms, bedrooms, and dens.

The 55-inch Bisbee ceiling fan celebrates the beauty of the natural world with the modern industrial styling of its woven, organic cage detail and contemporary technology from its integrated 20-watt LED light source. Damp-rated and powered by a state-of-the-art DC motor for indoor or outside covered areas, this ceiling fan embodies the art of tranquility.

Embracing a clean and uncluttered aesthetic, the Belen LED downrod ceiling fan focuses on simplicity and functionality. Three ABS blades meet to form the housing, which holds a quiet DC motor and an integrated 20-watt LED module.

The Insignia Three-Blade fan is a harmonious symphony of design and innovation. With a 60-inch size and three unique swoop-style ABS blades attached to a luxe metallic housing, this sleek fan effortlessly creates a breathtaking visual impact.

Want to go bigger? We also offer the Insignia Six-Blade, an impressive 72-inch size with windmill-style blades. Both fans come with a 3CCT integrated LED light kit offering three distinct lighting options - from warm, cozy hues to crisp, refreshing tones.
Explore new 2024 ceiling fans and more of the latest lighting collections here.