Showcase Your Home’s Personality with Statement Lighting
Progress Lighting describes how statement lighting is a conversations starter for the home, these fantastic styles express the homeowner’s personality and are the center of attention.

Written by Progress Lighting on March 31, 2022
It's often said that lighting is the "jewelry of the home." It's the finishing touch, the statement-maker, the wow factor. It's an incredible way to express your personality and add drama to a space. We like to think of statement lighting as "Conversation Starters." Our statement lighting creates a dialogue between two or more people: you won't have to worry about any awkward silences when guests enter your home and see your amazing lighting fixtures!
Sculptural forms, unusual design elements, large-scale sizing and brilliant finishes transform functional lighting fixtures into works of art. The tiny size of LED light sources, as well, has enabled lighting designers to create dynamic silhouettes that weren't possible with traditional incandescent bulbs.
Here are our picks for some of the best conversation-starting lighting to showcase your home’s personality and make maximum impact in your space.
The Radian LED Pendant defines a sleek contemporary style with an industrial vibe. A soft satin white domed metal shade is supported by a contrasting cap and is finished inside with a reflective soft satin gold coating that casts a warm glow of light from its integrated 30W LED module. The pendant's sleek design is ideal for any kitchen, breakfast nook or bar area in modern, contemporary, and mid-century modern style settings. It's also offered in two additional finishes: crisp black with a soft gold interior and a warehouse-inspired brushed nickel shade capped with black and soft gold within.
Ceiling mount lights create drama when hung in multiples down a hallway or on its own in settings like bedrooms, especially when they have a unique style. The Delayne Collection has a mid-century appeal defined by an array of arms with a star-like appearance that extends outward from a rounded, central support. Each spoke arm is tipped with an exposed bulb which can be customized with a round, candelabra or linear bulb, adding to the modern design and creating a soft ambient light. Select decorative light bulbs in a clear or white finish to further enhance this dynamic style. In addition, its sophisticated brushed bronze metallic finish interacts with the light, casting stunning reflections on ceilings.
Modern minimalism meets the future of industrial style in the Spoke Chandelier Light. Sleek rods coated in a beautiful matte black finish anchor the luminous circles for a retro yet contemporary vibe. Four slim disks of integrated LEDs cast an ethereal glow that creates a multi-directional wash of even light.
The League Chandelier distinguishes your home with a clean, modern design. Softly rounded squares interplay within each other as a modern take on a farmhouse cage chandelier. A beautiful matte black finish elevates the aesthetic, while classic etched glass shades emphasize the contrast between soft and clean.
Credit: Curate Homes and Piper Stromatt
Take a naturalistic approach to modern room design with the Mariposa Pendant. Slender branches bloom outward from the central stem bearing delicate leaves coated in a luxurious antique gold finish. The organic feel is balanced by the minimalist lines of its multi-directional light arrangement.
Learn more about unique lighting ideas to elevate your home’s style here.
Sign me up to receive the latest posts from the Progress Lighting Blog to my email.