Every year, more beautiful outdoor lighting fixtures come onto the market. New materials, LED light sources and other innovations mean that styles are trendier than ever. However, when choosing outdoor lighting, style is not your only consideration. The fixtures must be able to stand up to harsh weather conditions including salt air, bright sunshine, or areas that frequently experience high humidity or damp weather.
Featuring Benton Harbor
DURASHEILD Protected Outdoor Light Fixtures
That’s where DURASHIELD crafted outdoor lighting comes in. It’s Progress Lighting's innovative, durable material for outdoor lighting that is specially formulated to withstand the elements. Built to last, DURASHIELD is a corrosion-proof composite material with UV protection, creating a high-performance finish. DURASHIELD offers a 5-year warranty, meaning that fixtures constructed with DURASHIELD are protected from rust, corrosion and fading that can occur with adverse environmental conditions.
Here is a roundup of some of our latest outdoor light fixtures that feature DURASHIELD construction.
Jeffrey Alan Marks Point Dume™ Outdoor Wall Lantern Collection
Designer Jeffrey Alan Marks was inspired by one of his favorite places, East Hampton, NY for his exterior lighting collection. The pieces evoke thoughts of East Coast’s shimmering coastline and an authentic Americana vibe.
 |
The Wakecrest LED wall lantern brings an artful, rustic charm to often-seen utilitarian outdoor down lighting. It’s ideal scale and range of finishes make it suitable for various architectural styles ranging from cottage to contemporary: it’s a modern take on rustic luxury. Jeffrey translated the corrugated rooflines of classic barns into a softly waved sconce frame, paying homage to the Americana aesthetic. |
 |
With the Seamoor outdoor wall lantern, Jeffrey reinterpreted the elements of a traditional barn while maintaining a visual nod to the iconic originals. The wavy roof is inspired by a traditional corrugated metal roof yet is more playful with its undulating curves. The handle is reminiscent of those found on old wall lanterns, but its square shape adds a contemporary interpretation. |
 |
The Hook Pond outdoor wall lantern features a steeply pitched, barn-inspired roof crowned with a distinctive loop finial. Hook Pond offers a contemporary edge on traditional corrugated metal barns found throughout the East Coast. |
 |
The Dunemere outdoor wall lantern has a playful silhouette reminiscent of a classic barn and modern A-Frame architecture. It’s casual and rustic, perfect for both indoor-outdoor rooms from Urban Cottage to Farmhouse style homes. |
New Outdoor DURASHIELD Protected Light Fixtures
New fixtures in the Progress Lighting line constructed from DURASHIELD capture an updated traditional aesthetic that’s ideal for creating curb appeal in homes from coast to coast.
The Gables outdoor wall lantern Collection elevates your home decor with the graceful arches of an outdoor hanging lantern light. The lantern's stately frame is coated in a crisp satin white finish and a light source glows from within clear glass.
Partner timeless elegance with a pinch of coastal vibe with an outdoor hanging lantern light from the Grandbury outdoor wall lantern Collection. A beautiful square frame crafted from corrosion-proof composite polymer material features a half loop on top of the structure and is accented by crisp, clear glass panes.
Want to ensure your outdoor lighting is protected? Explore our full range of outdoor light fixtures crafted from DURASHIELD.