Today's Trends: New Looks in Ceiling Fans

Ceiling fans are good for more than simply cooling a room - they've become a welcome addition to defining your home's style. With gorgeous new designs, ceiling fans can be as statement-making as a chandelier centerpiece in a room and become the star of the room's design - while still providing the latest in energy efficiency and control.

Before selecting your perfect ceiling fan design, begin by collecting the proper measurements. Determining ceiling height is critical - after hanging the fan, the fan blades should be a minimum of 7 feet from the floor, and 8 or 9 feet of clearance is even better. For ceilings over 9 feet, plan to purchase a ceiling fan with a down rod option to achieve the perfect hanging height.

Next, make sure to choose a fan that has a diameter that is proportional to the size of the room. Basic guidelines are:

  • Rooms up to 75 square feet, select a 29 to 36-inch diameter fan
  • Rooms 76-144 square feet, select a 36 to 42-inch diameter fan
  • Rooms 144-225 square feet, select a 44 to 50-inch diameter fan
  • Rooms 225-400 square feet, select a 50 to 54-inch diameter fan

Now for the fun part: choosing a fan that fits the personality of your space! The possibilities are virtually endless, with a wide range of styles that are ideal for indoor and outdoor locations.

Today's fans often feature unique design elements that complement the design intent of the room. Look for watermarked and etched glass bowls, hand-carved wooden blades, sleek metal accents, blades with washed finishes, and even canvas-wrapped blades.

Same room with three different looks. Ceiling fans can be a great statement piece in achieving a refreshed look.

When it comes to cooling down your home this summer, we've got you covered. Here are some of our top picks from our ceiling fan line that reflect the latest trends:

Sanford, with its "fandelier" styling and metal-banded cage enclosing the light source, offering a vintage Industrial look.

The carved-wood blades of Farris are ideal for Modern, Contemporary and Industrial settings.

Edisto, with a wire frame supporting canvas-wrapped blades featuring UV inhibitors to protect the fabric from fading in the sunlight is perfect for outdoor locations

Braden, a hugger-style ceiling fan with sleek fan blades finished in clean metallics for a design that complements Modern interiors.

The statement-making, Springer Twelve-Blade fan is inspired by the form and function of a windmill and is ideal for Farmhouse, Industrial and Transitional interior settings.

There truly is a ceiling fan to fit everyone's decor style. For more inspiration, shop Progress Lighting ceiling fans here.



Recommended Posts

Ceiling Fan Season

It’s Ceiling Fan Season!

Continue Reading

Get the Look: Mudrooms with Style

Continue Reading
Front Porch Styling Tips for Springtime

Front Porch Styling Tips for Springtime

Continue Reading