Sleep in Style: Explore the Top Bedroom Lighting Fixtures
Discover Progress Lighting’s tips for creating a bedroom that is a peaceful sanctuary using inspirational design and a guide to the best bedroom lighting.

Written by Progress Lighting on April 28, 2023
Bedrooms today are more than a place to enjoy a good night's sleep. It is where we start and end the day, it can do double duty as an office, or it can serve as a restful retreat and an escape from daily life. Here is a roundup of inspiring design and lighting tips to create a haven you will love spending time in.
Modern and organic inspirations elegantly meld together with clean lines, minimal decoration, and a connection with nature. Emphasize the environment with large windows that offer relaxing views of the outdoors. Layered neutrals, warm-washed woods, and matte black accents bring a naturalistic vibe while completing the serene feel of this mountain retreat.
Select a light that brings a mid-century modern flair to the bedroom. The Haas chandelier has a bold linear frame that branches out to embrace etched glass globes, imbuing a space with soft illumination. To free up room on bedside tables, install wall sconces on either side of the bed. The Hinton swing arm wall light has an opaque matte black metal shade and signature adjustable arm ready to provide focused task light wherever illumination is called upon, making it a favorite choice for reading a favorite novel before bed.
Add boho charm to a bedroom with loads of textures that offer an international appeal. A minimalist approach combines sleek elements and patterned décor, offering a pop of color. The key to this style is that by keeping it intentionally personal, with a "gathered over time" look, it becomes relaxed, carefree, and inspiring.
Select a rustic ceiling fan like Bastrop, whose updated vintage styling comes from its wood tone and metal cage frame construction. Curved fan blades in distressed wood feature an interesting bend that heightens the fan's industrial aesthetic.
Provide sophisticated task lighting with a pair of Galloway wall sconces above a desk. Clean, modern lines combine with rustic elements and a candelabra light that glows brightly to illuminate the surface in a casually elegant style.
Stay calm, relaxed, and collected in this peaceful space. A lovely blue and white scheme soothe the senses while adding a breath of fresh air with a pop of bright blue. This coastal-inspired home is all about being soft and bright.
Make a statement on your ceiling with the Atwell semi-flush mount light. It anchors the space with a central stem finished in mellow brushed bronze capped by clear glass globes delivering the perfect amount of ambient illumination.
Use warm gold tones for cabinet pulls, art frames and lighting finishes to create a soothing yet vibrant vibe against the white walls of this room. Touches of wood help soften the edges of a contemporary neutral color palette. This bedroom is replete with weathered wood furnishings that take a minimalist room design and layers on texture for visual interest.
A lustrous vintage brass finish showcases the elegant design of the room's lighting. The airy Gilliam chandelier delivers an ethereal quality from its slim circular silhouette highlighted by traditional, simple candle slips. A pair of Gilliam pendant lights hung on either side of the bed complement the rich tones of the room, while a clear glass shade enhances the ceiling light's classic form while providing task illumination.
Feeling inspired for your bedroom lighting upgrade? Shop all the best bedroom fixtures on our website.
Sign me up to receive the latest posts from the Progress Lighting Blog to my email.