PROGRESS LIGHTING
PROGRESS LIGHTING

Quick Tips with Chris Primous - Part 3

Chris Primous is the Vice President of OEM sales and Industry Relations at MaxLite. He is a recognized energy-efficient lighting industry expert, educator, and champion for the lighting manufacturing industry with programs such as ENERGY STAR, California Title 24 and Title 20.

How do I know what LED wattage is the best replacement for incandescent, halogen, or CFL bulbs?

The first step is to remember that wattage does NOT equal light output. The historical use of incandescent bulbs has conditioned many consumers to believe that light output is equivalent to wattage. Therefore, many consumers believe that a 60W incandescent bulb needs to be replaced by another 60W bulb. Actually, wattage shouldn't be the deciding factor when trying to figure out if a light bulb has the proper light output needed. LUMENS is the proper measure of light output, and should be the primary factor in determining if the selected bulb has enough light output for the intended use. Since LEDs are more efficient than incandescent (and most other lighting technologies) at converting electrical power to lumens, the actual wattage needed to create the necessary amount of light is quite low in comparison, and decreasing each year as LED technology becomes even better. Whereas a 60W incandescent bulb typically produces 800 lumens (abbreviated "lm") of light, similar LED bulbs in 2018 require only approximately 9W of power to produce the same 800 lm. Thus, the replacement for your 60W incandescent bulb would be a 9W LED bulb. LED technology is still becoming more efficacious, so in the short future, this same 800lm can likely be produced by a 7-8W or lower LED bulb. It is important to know what lumen level you are trying to replace, and by knowing that info, you can properly select the best LED replacement. Most LED bulb manufacturers will state which common incandescent bulbs their LED bulbs can typically replace on their packaging and in marketing literature. LED lamp equivalents will vary by manufacturer and product type, but for the most common types of bulbs such as everyday Omni A-19 lamps, today the equivalents would approximately be:

40W INC = 450lm = 9W CFL = 6W - 7W LED 60W INC = 800 lm = 13W CFL = 7W - 10W LED 75W INC = 1100 lm = 18W CFL = 11W - 12W LED 100W INC = 1600lm = 23W-26W CFL = 14W-17W LED

Not sure just how much a bulb can make  difference?

See for yourself in our quick round up of new lighting fixtures that complement the best that affordable luxury living has to offer.


Recommended Posts

 New Oscillating Fandeliers and Ceiling Fan Design Trends

New Oscillating Fandeliers and Ceiling Fan Design Trends

Continue Reading
New 2024 Lighting Designs

Sneak Peek: New 2024 Lighting Designs

Continue Reading
5 reasons you should treat yourself to new lighting

5 Reasons Why to Treat Yourself to New Lighting

Continue Reading