When specifying a foundation system, one of the most common questions engineers, utilities, contractors, and owners ask is: "How long will it last?"
For steel foundations, the answer often centers around corrosion resistance and long-term performance in real-world soil conditions. Fortunately, Chance® Instant Foundations are backed by decades of field experience and documented installations that demonstrate exceptional durability.
Evaluations of foundations installed in the early 1980s reveal that hot-dip galvanized Chance Instant Foundations continue to provide reliable structural performance after more than four decades in service.
Unlike paint coatings that can be damaged or peel over time, galvanized zinc acts as a sacrificial anode that protects steel by corroding first. This sacrificial action helps preserve the structural steel beneath and significantly extends service life in a wide range of soil conditions.
Galvanized coatings provide:
Not all soils are equally corrosive. Two key indicators help predict the corrosion potential of buried steel foundations:
Second, soil pH helps predict foundation longevity. Soils with a neutral pH near 7 are generally less corrosive than acidic soils with pH values near 5 or below.
According to Chance engineering guidance, well-draining soils with resistivity levels above approximately 2,000 ohm-cm can typically support a service life exceeding 50 years. That estimate does not mean the galvanizing is fully consumed after 50 years; rather, it indicates that expected material loss is generally not enough to compromise structural performance.
One of the most compelling examples comes from a Chance Instant Foundation installed in December 1983 at the Gibson Substation in Centralia, Missouri.
The foundation remained in service for more than 32 years before being excavated and analyzed in March 2016. Researchers evaluated galvanizing thickness, examined corrosion patterns, and inspected the steel for material loss.
The installation site included:
These conditions represent a demanding environment for any buried steel foundation.
After more than three decades underground, inspectors found:
Galvanizing still present on the foundation
Minimal corrosion on the upper and middle shaft sections
No significant steel loss affecting performance
Corrosion concentrated primarily near the lower shaft, helix, and base plate regions
Continued structural integrity of the foundation system
Researchers noted that discoloration visible on portions of the excavated foundation was not rust; when scratched, galvanizing remained present beneath the surface layer.
Historical galvanizing thicknesses for the foundation were estimated between 5 and 7 mils. Upon removal and inspection, measurable zinc remained across the foundation after more than three decades in service.
Using the most conservative measurements, engineers calculated a zinc loss rate of approximately 0.19 mils per year.
This result indicates exceptionally slow corrosion progression, even under relatively challenging soil conditions. At that rate, galvanized protection continues to provide decades of service before the underlying steel becomes exposed.
The Centralia corrosion study is not an isolated example of long-term performance.
Chance documentation also references transmission line foundations installed in Minnesota’s Tamarack Swamp in 1977, providing another long-term field example in a challenging soil environment.
The following photos show Chance foundations in Centralia, Missouri, that are still in use today. Based on the best available information, they were originally installed in the late 1960s, meaning they have been in service for more than 50 years. Zinc remains visible on the base plate, reinforcing the long-term durability demonstrated by these field installations.
These installations provide real-world confirmation that galvanized Chance foundation systems can deliver reliable performance over multiple generations of infrastructure.
As with any foundation system, expected service life should be evaluated using project-specific soil data, environmental exposure, loading requirements, and applicable engineering guidance. When evaluating foundation alternatives, life-cycle performance is every bit as important as initial installation cost.
The combination of:
gives engineers confidence that Chance Instant Foundations can provide dependable long-term support for lighting, utility, telecommunications, signage, and other infrastructure applications.