Progress Lighting Blog

Understanding Color Selectable LED Lighting

Written by Progress Lighting | Jan 28, 2021 5:00:00 AM

There's no doubt that new LED technologies have entered our lives, and quickly. This year, we've introduced a new portfolio of color selectable LED fixtures. Understanding color selectable LEDS means understanding the basics of color measurement to help you in your search for the perfect light color for your room.

Color selectable fixtures have LED light sources built right into them. "Selectable" means that there are multiple distinct white light settings within the LED. With just a flip of a switch, color selectable LEDs can change between pre-set color temperatures of white light, from warm to cool settings. Color selectable should not be confused with tunable white, which blends white colors along a continuous scale. Lastly, it is not RGB or RGBw, which uses red, green, blue and/or white to create colors other than white.

Distinguishing and Defining Color
Here's a quick primer on the basics of color metrics: correlated color temperature (CCT), the color rendering index (CRI) and the Kelvin scale (K), and how they work together to give you the best possible light for your room application.

Kelvin Scale (K)

The color temperature of light is measured in Kelvin. The lower the Kelvin number, the warmer the light will appear. Warm, or yellow light measures lower on the scale (typically 2000K- 3000K) and creates a cozy, relaxed mood in a room. Lights that measure 3100K - 4500K create a more energetic mood in a room. Color temperatures from 4600K - 6500K offers a crisp white light and are ideal for environments where more light is required.

Correlated Color Temperature (CCT)

CCT refers to the visual appearance of white light. White light can appear either warm (more yellow) or cool (bluer). Warm light corresponds to a lower CCT on the Kelvin scale, and cool light measures higher on the Kelvin scale. This color influences the appearance or mood of the spaces in which artificial light sources are used. Warmer light is ideal for living rooms and bedrooms; cooler light is perfect for bathrooms, workspaces and outdoor security lights.

Color Rendering Index (CRI)

CRI is a measure of light quality on a scale of 1 and 100. It measures color perception or how accurately colors are visually perceived compared to a natural light reference source. Simply said, a higher CRI value offers better color rendering: the colors will show truer and can appear more saturated, as opposed to appearing washed out or faded. In general, look for a CRI over 80. A CRI of 90 or more offers very accurate color rendering.

Advantages of Color Selectable Fixtures
Choosing color selectable LED fixtures offers design flexibility and the ability to control lighting within multi-functional spaces.

Design Flexibility
Color selectable fixtures empower lighting designers and customers to customize lighting based on the room's decor intentions. With color selectable lighting, it's easy to install the lights first, and then select the perfect color temperature for the room setting. The room's ambiance can be changed, for example, depending on the time of day or the mood you want to set.

Lighting Multi-Functional Spaces
Today's rooms are used for many functions. With color selectable LED lighting, you can select the light level depending upon what's happening in a room at any given moment: the choice is yours.

Color Matching
If you are adding lights to a room, with color selectable fixtures, it's easy to set the color temperature to match the existing light fixtures. This creates a cohesive look to the space.

Adaptability
Color Selectable fixtures allow users to change settings in the future should the need arise based on preference changes, space redesign, adaptation to added sources or furnishings, or adaptation to age.

Check out some of our new color selectable fixture styles: the Intrinsic collection, Hide-A-Lite linear undercabinet lighting, the Everlume collection and more!

Shop all new 2021 Progress Lighting fixtures here.