Three popular places to install statement lighting, the "wow" pieces that express your home's style and personality, are over kitchen islands, dining room tables, and entrance foyers. And there are plenty of fantastic fixture options to enhance those spaces while providing plenty of light for guests and family.
Frequently asked questions include what size fixture to buy and how high to hang fixtures. Here are some sizing and hanging heights guidelines for kitchen islands, dining room tables and foyer.
Featuring Gulliver
Chandeliers over the dining room table usually provide a dramatic focal point and task and general lighting for the room. Use the table under the chandelier to serve as a guide for selecting the chandelier's size by measuring the width of the table and subtracting 12 inches. For example, if your table is 42 inches wide, your chandelier should not be more than 30 inches wide. The bottom of the chandelier should hang between 30 to 36 inches above the table.
Featuring Kempsey
You can also design a chandelier using three or more pendants hung at varying heights over a dining room table by purchasing a canopy kit. These kits allow 3 to 6 pendants to be hung together in a line or a circular group. Or install the pendants individually to create a custom lighting design.
WATCH: Chandelier hanging heights and sizing tips |
Featuring Parkhurst
Pendants are versatile lighting options for many rooms in your home. Smaller-scale "mini-pendants" look great when hung in groupings of 3 or more over a kitchen island or table. Medium and large pendants can be hung in pairs to make a dramatic statement. To size pendants, keep in mind that pendants should be at least 10 inches smaller in diameter than the width of the countertops.
To install pendants over kitchen islands:
WATCH: Pendant lighting trends and sizing tips |
Chandeliers, pendants, convertible fixtures and semi-flush mount fixtures are popular choices for foyers. These fixtures have the light source, shade and other decorative elements suspended from the ceiling by rods, chains, or additional extensions. The resulting gap between the light and the ceiling offers a visually dynamic effect.
Select the foyer light's size by adding the length and the width of the room together (measured in feet), then converting that measurement to inches. For example, a 10 x 10 foyer equals 20 feet, which translates to a fixture size of approximately 20 inches in diameter.
As a rule, keep 7 feet of clearance from the floor to the bottom of the fixture because people may walk underneath it. If your ceiling is higher than 11 feet, divide the vertical space into thirds, positioning the chandelier two-thirds of the distance from the floor.
WATCH: Close-to-ceiling lighting trends and hanging tips |
Discover more lighting fixture sizing and hanging guidelines here.