As we age, so do our eyes. Physical changes take place that makes seeing everyday objects and performing everyday tasks more difficult. The eye's lenses begin to discolor, making it harder to see and distinguish between certain color shades. The muscles that control pupil size and reaction to light lose some strength, so glare becomes an issue. Other changes cause light entering the eye to be scattered rather than focused precisely on the retina, affecting vision quality.
Proper lighting can help alleviate some of these issues. Here are some ways to make the right lighting choices to ensure a safe, healthy and independent way of living as we age.
Image courtesy of GreenTech Homes & Piper Stromatt. | P500147-109-30
Choose LED Lights
One of the best ways to begin is to select LED light sources whenever possible. Choose fixtures that have LED lights integrated inside them or replace existing light bulbs with LED bulbs. LEDs offer a range of color temperatures, from cool to warm. As our eyes age, it is easier to perceive cooler colors than warmer ones. LED lights are available in specific color temperatures, such as 2700K - 3000K, a warmer range and 4000K and higher, which are cooler. And new LED technology is now available that offers color-changing abilities within the bulb itself, so color temperatures can be precisely controlled to a color that works best for the individual and the space.
Image courtesy of Stephen Alexander Homes. | P500047-104, P700005-028-30 and P700003-028-30
More Tips for Aging Vision
The Illuminating Engineering Society offers additional lighting guidelines for the aging eye, including:
Shop our wide selection of lighting and accessories here.