Just like dressing in layers is necessary for the fall, light must be layered to create a cozy and functional ambiance. The key to a proper lighting plan is to use a multi-layered approach that combines three types of light: ambient, task, and accent lighting.
Ambient lighting is the foundational, general illumination that typically comes from overhead fixtures like chandeliers and flush mounts, plus natural light from windows. Think of it as the practical light of the space.
Task lighting provides directional light on specific work areas or tasks. Pendants, recessed lights, and undercabinet lighting are all excellent choices for task lighting.
Accent lighting from wall sconces creates visual interest and adds drama to a room. Use it as part of an interior design scheme to highlight a room's decorative features, architectural details, and other focal points. Accent lighting should be three times brighter on the focal point than the general light surrounding it.
Credit: Stephen Alexander Homes
Start your lighting plan in the kitchen, which is typically the most-used space in the home. Select ambient lighting first. Select recessed, cove, soffit, or linear lights to provide soft illumination. For a traditional look, use overhead flush mount ceiling fixtures or a chandelier.
Since ambient light comes from everywhere, including natural light, it provides the light for general navigation throughout the room. However, this overhead light often leaves shadows that interfere with the light needed to perform cooking, reading, and other tasks effectively. This is where task lighting comes into the plan.
For task lighting, begin with the light for work areas. Since upper cabinets tend to block light, install undercabinet lighting, such as puck lights or tape lights, for direct lighting on the countertops. Try smaller pendant or recessed lights to add task illumination over the kitchen sink or cooking surface. Use several larger pendants to highlight the kitchen island. Finally, add toe kick lighting along cabinet bottoms to create a clearly lit path at night.
Then, select statement-making chandeliers and pendants to define dining and living areas and create interest points for each zone. As the final flourish to the design, layer in accent lighting: wall sconces, table, and floor lamps for added ambiance.
Find the perfect lighting for all light layers here.