Progress Lighting Blog

Enhance Your Décor with the Best New Ceiling Fans

Written by Progress Lighting | Jun 15, 2023 8:29:13 PM

This summer, enhance your decor with ceiling fans that do more than provide cooling breezes. Express your personality with selections from our latest ceiling fan collections that epitomize the newest interior design trends. Progress Lighting’s new ceiling fans for 2023 deliver on style and are guaranteed to bring your space to life this summer and for the seasons beyond.  

Modern Organic Style


Modern organic styling uses authentic, sustainable, and eco-friendly materials along with curved lines, rounded edges, and asymmetrical patterns, creating a sense of fluidity and naturalness in the design of the Schaffer II fan. Nature-inspired themes remain popular, and fan design reflects this, with hand-carved blades finished in warm wood tones. In addition, unusual materials like wicker and jute are used to accent fan housings, creating a layered and textured look that invites comfort and offers a global flair.

"Relax in the cool breezes of our new, world market/global design trending ceiling fans," said Steve Register, Progress Lighting Sr. Product Manager "With a natural jute rope wrapping around the motor and another with a wicker basket surrounding the LED light, these fans are perfect indoors or outdoors in a damp location and will enhance any cottage/coastal décor."


Bring a global presence to ceilings with the Schaal fan, which features a unique, wicker-wrapped shade and five reversible fan blades. The Schaffer four-blade ceiling fan showcases natural jute rope wound around its housing, softening its look.  


Unique metal detailing on the blades of the Bexar ceiling fan join to form a flower-like pattern, bringing a touch of whimsy to modern homes. The Dallam ceiling fan continues the floral theme by graciously creating the impression of a flower in bloom as its six blades wrap around gently around its opal white shade.  

Celebrate Contemporary Design


Effortlessly create a high-end space with ceiling fans that celebrate contemporary style. These fans move away from blocky, traditional fan blades into sleek shapes made possible using materials like ABS. This plastic is easily molded into aerodynamic shapes that move a lot of air. Fan blades are detailed with metal straps, bars and other geometric shapes to add to their cool look. For example, our new Brazas 56-inch ceiling fan features six ABS fan blades fashionably detailed with bracketed trim, and a quiet and energy-efficient DC motor to keep spaces cool in style.

Incorporate Innovative LED Technology


Some new fans incorporate integrated LED modules with color temperature selectability. This innovative technology means your fan can cast a low, romantic light or dial up the color temperature for cheerful bright, crisp illumination. A clean, modern design and color-selectable LED technology give the Tarsus 52-inch ceiling fan high function and a distinctive style.

"Putting color selection in your hand is as simple as a press of a button on your remote control," points out Steve. "Select from a warm 2700K, a soft white 3000K, or a 5000K bright white light - you can either set it and forget it or select a different color light as often as you wish."

These fresh new fan designs and more debut next week at Lightovation, the International Lighting Show, in Dallas, and will be available soon from retailers across the country and online. Find out where to buy near you here. Or shop ceiling fans online.