---
title: Reduce Installation Errors with SureFit™ Aluminum Automatic Splices
description: The SureFit automatic splice was designed to minimize partial insertion errors, the most common failure with automatic splices.
---

[Hubbell Power Systems Blog ](https://blog.hubbell.com/en/hubbellpowersystems)

# [Reduce Installation Errors with SureFit™ Aluminum Automatic Splices](https://blog.hubbell.com/en/hubbellpowersystems/reduce-installation-errors-with-surefit-aluminum-automatic-splices)

 Written by [Kimberly Thomas](https://blog.hubbell.com/en/hubbellpowersystems/author/kimberly-thomas) | Aug 30, 2018 1:37:00 PM

The SureFit™ automatic splice was designed to minimize partial insertion errors, the most common failure with automatic splices. On other splices, partial insertion may occur during installation when the conductor has not completely passed through the jaws, reaching the area of the center stop. 

Hubbell Power Systems, Inc. has a patented insertion mitigation design, which prevents the jaws from engaging and biting down on the conductor until it is fully inserted.

**A Clear Path**

The SureFit [automatic splice ](https://www.hubbell.com/hubbellpowersystems/en/Products/Power-Utilities/Connectors/cl/548025)sets itself apart from other splices. First, the SureFit splice includes a longer funnel guide and longer pilot cup, which allows a clear path for the conductor to reach the jaws. This makes conductor insertion much smoother, especially when using larger size conductors

**The Hollow Chamber**

Also, SureFit automatic splices have a high density plastic pilot cup which has a hollow chamber, that allows the conductor strands to stay in place, minimizing the chance of errant strands, and a solid chamber that sits within the jaws allowing them to remain open without deforming the pilot cup.

**Positive Insertion Indicator**

Lastly, the funnel guide indicator is an indispensable feature of the SureFit splice. The funnel guide indicator will only deploy upon full conductor insertion meaning the conductor has to completely pass through the jaws. The jaws will then close and the high strength spring pushes the jaws forward, and triggering the funnel guide indicator to deploy. When the funnel guides deploy full conductor insertion has been achieved.

The SureFit splice is offered in a wide range of sizes and is available in a corrosion-resistant version. The SureFit splice ensures that installation is done correctly, whether used for storm restoration or routine maintenance. For further explanation, watch the SureFit In-Depth video.

[View full post](https://blog.hubbell.com/en/hubbellpowersystems/reduce-installation-errors-with-surefit-aluminum-automatic-splices)

```json
{
  "@context" : "http://schema.org",
  "@type" : "BlogPosting",
  "author" : {
    "@type" : "Person",
    "name" : "Kimberly Thomas"
  },
  "dateModified" : "2025-01-09T16:05:44.744Z",
  "datePublished" : "2018-08-30T13:37:00Z",
  "headline" : "Reduce Installation Errors with SureFit™ Aluminum Automatic Splices",
  "image" : {
    "@type" : "ImageObject",
    "height" : 687,
    "url" : "https://cdn2.hubspot.net/hubfs/2897803/Content%20Campaigns/Connectors/AS4-302293-edited.jpg",
    "width" : 904
  },
  "mainEntityOfPage" : "https://blog.hubbell.com/en/hubbellpowersystems/reduce-installation-errors-with-surefit-aluminum-automatic-splices",
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
    "name" : "Hubbell Power Systems Blog"
  }
}
```