---
title: Not All Polymer is Created Equal | Hubbell's Polymer Insulators Educational Series
description: Discover the complexities of polymer compounding for utility electrical equipment. Learn how materials, additives, and design impact performance, and explore Hubbell's proprietary polymer compounds for high voltage insulators.
---

[Hubbell Power Systems Blog ](https://blog.hubbell.com/en/hubbellpowersystems)

# [Not All Polymer is Created Equal | Hubbell's Polymer Insulators Educational Series](https://blog.hubbell.com/en/hubbellpowersystems/not-all-polymer-is-created-equal)

 Written by [Jeff Butler](https://blog.hubbell.com/en/hubbellpowersystems/author/jeff-butler) | Oct 26, 2021 7:00:00 PM

Polymer compounding for utility electrical equipment is a complex subject. Too often, [insulators](https://www.hubbell.com/hubbellpowersystems/en/Products/Power-Utilities/Insulators/cl/560222) are dismissed as commodity products. The perception that the base polymer alone defines all product characteristics is mistaken. Nothing could be further from the truth. Materials (including additives and fillers) and design impact performance.

Today we want to give you some background and introduce our two proprietary polymer compounds:

- [Why silicone for HV insulators: Silicone compounds explained](https://blog.hubbell.com/en/hubbellpowersystems/why-silicone-for-hv-insulators-silicone-compounds-explained)
- [ A look at silicone compounds for HV insulators: Testing performance](https://blog.hubbell.com/en/hubbellpowersystems/hubbellpowersystems/a-look-at-silicone-compounds-for-hv-insulators-testing-performance)
- [ Hubbell’s proprietary ESP™ polymer explained](https://blog.hubbell.com/en/hubbellpowersystems/hubbellpowersystems/hubbells-proprietary-esp-polymer-explained)
- [ Why Hubbell Quadri*Sil® insulators provide longer life](https://blog.hubbell.com/en/hubbellpowersystems/why-quadrisil-insulators-provide-longer-life)
- [ Considering insulator equivalence? Polymer versus porcelain](https://blog.hubbell.com/en/hubbellpowersystems/how-to-choose-a-polymer-insulator-equivalent-for-a-porcelain-string)

This series will give you a solid understanding of polymer compounds for high voltage insulators. The information will help you choose the best material and design for your application.

## **Background Experience in Polymer Insulators**

Hubbell’s long history of innovation has played an important role in the development of high-voltage insulators. In the late 1880s, the [Ohio Brass company](https://www.hubbell.com/hubbellpowersystems/en/hps-brands/ohio-brass) was founded about the same time as Hubbell Incorporated.

Ohio Brass was a leader in the [porcelain insulator](https://www.hubbell.com/hubbellpowersystems/en/Products/Power-Utilities/Insulators/Station-Post/Porcelain/c/561326) industry, patenting the original cap and pin porcelain insulator design still commonly used today. Our porcelain bell insulators were used in the first high voltage transmission line in North America, at Niagara Falls in 1905.

In the 1960s, the industry was investigating polymer compounds as an effective alternate material for insulators to support the expanding power grid. Polymer materials offer a viable alternative to porcelain for several reasons:

- weight savings
- improved performance in contaminated environments
- added safety
- increased design versatility

By the time Ohio Brass became part of the Hubbell family in 1978, we had been researching polymer technology for almost 14 years. The success of our early Hubbell polymer insulators helped fuel the growth of the market segment.

## **A Tale of Two Polymers**

The result of almost 60 years’ experience of successful development, testing, and field deployment has been the creation of two proprietary polymers for high-voltage insulators. These offer you different feature characteristics that deliver superior performance in the harshest environments. For a quick overview, see our[ comparison page](https://hubbellcdn.com/ohwassets/HPS/literature/AD08069E_TD_ESPVSilicone.pdf).

<https://hubbellcdn.com/literature/AIK-INSUL-SF-EN-02785.pdf>Our proprietary [silicone rubber](https://hubbellcdn.com/literature/AIK-INSUL-SF-EN-02785.pdf) is compounded with a 100% silicone base. Silicone provides excellent hydrophobicity (the ability to repel water) and UV resistance to the insulator. However, more is required to protect an insulator throughout its life. Additional components are needed in the compound to deliver other characteristics. These include superior tracking resistance and corona resistance—ours is 10X greater than typical silicone compounds.

Combined with effective insulator designs, these characteristics of our silicone rubber extend the life of the insulator and combat the damaging environment of high voltage insulator applications.

<https://hubbellcdn.com/literature/AIK-INSUL-SF-EN-02706.pdf>Our proprietary [ESP™ enhanced silicone polymer](https://hubbellcdn.com/literature/AIK-INSUL-SF-EN-02706.pdf) is a blend of silicone base and ethylene propylene diene monomer (EPDM). A key benefit is its greater mechanical strength and durability. ESP polymer offers 3X more tear strength than commonly available silicone polymers. Along with excellent tracking resistance and hydrophobicity, it provides exceptional UV resistance--lasting over 8X longer than ASTM test requirements. ESP material is also bird and rodent resistant, making it perfect for applications where animal contact may be a concern.

Both exclusive polymers provide high reliability and long-term durability that critical high voltage insulator applications require. Hubbell offers an extensive line of polymer insulators for both [transmission](https://www.hubbell.com/hubbellpowersystems/en/markets/transmission) and [distribution](https://www.hubbell.com/hubbellpowersystems/en/markets/distribution) voltages. 

## **Next: Get an Inside Look at Compounding**

Not all polymers are the same. Hubbell’s compounding and design experience deliver performance and options beyond meeting the required standards for utilities worldwide. Read the [blog post](https://blog.hubbell.com/en/hubbellpowersystems/why-silicone-for-hv-insulators-silicone-compounds-explained) now.

[View full post](https://blog.hubbell.com/en/hubbellpowersystems/not-all-polymer-is-created-equal)

```json
{
  "@context" : "http://schema.org",
  "@type" : "BlogPosting",
  "author" : {
    "@type" : "Person",
    "name" : "Jeff Butler"
  },
  "dateModified" : "2025-06-17T18:38:35.845Z",
  "datePublished" : "2021-10-26T19:00:00Z",
  "headline" : "Not All Polymer is Created Equal: Discover Hubbell’s Proprietary Compounds",
  "image" : {
    "@type" : "ImageObject",
    "height" : 628,
    "url" : "https://2897803.fs1.hubspotusercontent-na1.net/hubfs/2897803/FINAL_IPC_Not-All-Polymer_smadv_1200x628px-no-logo.png",
    "width" : 1200
  },
  "mainEntityOfPage" : "https://blog.hubbell.com/en/hubbellpowersystems/not-all-polymer-is-created-equal",
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
    "name" : "Hubbell Power Systems Blog"
  }
}
```