A common question asked by engineers and contractors is “how does anchor spacing affect uplift and/or compression capacity of helical anchors and piles?” Most building codes require a reduction in axial capacity for pile spacings closer than 3 pile diameters on center. This is known as group effects. Codes further state group effects shall be evaluated using a generally accepted method of analysis. The “standard rule” for center-to-center anchor/pile spacing used by Hubbell Power Systems engineers is an S/B ratio of 5, where the “B” is the diameter of the largest helix plate; and a minimum spacing no less than 3 FT.
This article reviews the current level of research on the effects of anchor spacing on both tension and compression capacity of helical foundation elements like anchors and piles. The research is on-going, but there is considerable work done by others, plus the current research being conducted by Hubbell Power Systems. The objective is to develop a “generally accepted method of analysis” that is simple to apply to a variety of applications and site conditions.
Interaction of Multiple Helical Earth Anchors Embedded in Granular Soil conducted small-scale model tension tests on in-line anchors and groups. Their results indicate the critical horizontal spacing (S/B) ratio of single-helix anchors in dense sand appears to be > 5.
Axial Uplift of Square-Shaft Single-Helix Anchor Group conducted full-scale tension tests on pile groups in both hard and soft clay at the same location. The overburden soils were hard clay, and the soft to firm clays were deeper. The results indicate the critical horizontal spacing (S/B) ratio of single-helix anchors in hard clay appears to be > 4. Likewise, full-scale tension tests on pile groups indicate there is no critical horizontal spacing (S/B) ratio of single-helix anchors in soft to firm clay.
Field Study of Group Effects on the Pullout Capacity of “Deep” Helical Piles in Sand conducted full-scale tension tests on pile groups in loose to medium-dense sand. Their results indicate group efficiencies ranging from 60% - 95% for single-helix anchors in loose to medium-dense sand with S/B ratios of 2 – 3.
CHANCE engineers have recently conducted anchor spacing research in both clay and sand soil profiles. The clay site was in Centralia, MO, which has a medium to stiff clay soil for the top seven to ten feet. Full-scale tension tests on in-line anchors indicate the critical horizontal spacing (S/B) ratio of single-helix anchors in medium to stiff clay appears to be > 2. The group efficiency trends from about 89% at S/B of 1 to nearly 100% at S/B of 4. Figure-1 is a plot of the actual group efficiency values as a function of S/B ratio and the associated trendline.
Read more about pile and anchor design methodology in Section 5 of the Civil Technical Design Manual.
The current and past research generally follows the same trend. Both past and current research confirms that critical horizontal spacing (S/B) ratio is affected by soil type and relative density/consistency:
Research is ongoing. Our engineering experts will provide updates as relevant.