MY LISTS
GAI-TRONICS
GAI-TRONICS

Clean Room Communications

Clean Room Communications | Blog

What Goes Into Clean Room Communication?


In today’s interconnected world, Clean Rooms cross many vertical markets, including the healthcare, food processing, education, biotech and pharmaceutical industries. With the spike in popularity of the pre-fabricated “clean room in a box” and other types of portable clean rooms made by various clean room manufacturers, there are steadily increasing numbers of clean rooms being installed across the globe. Although the purposes of the rooms may vary, certain requirements remain constant: it is critical that the products going into clean rooms must be 100% reliable and it’s imperative that they are be able to withstand these frequently harsh environments.


Products like our Clean room telephones have proven themselves in the clean room environment for over thirty years. Transitioning from analog versions to newer VoIP models has allowed these phones to evolve with today’s technology. Design features include large buttons with clearly marked functions that are easy to find if an emergency occurs, an auto-answer feature and automatic call diversion. Add our TMA software to view and report the health of our Clean Phones and you’ve got a no-fail, easy-to-operate method of communication between the clean room and the outside world.


So, what about the necessary durability? Also proven over the past three decades! The smooth front panel of our market-leading design is sealed with a graphic overlay that keeps the phone particulate-free while also protecting it from the exposure of widely used clean-room chemicals like bleach and isopropyl alcohol. Actually, these phones can withstand exposure for more than 24 hours to over 60 different chemicals!


Other than a clean room facility, a clean room phone could also be installed in the following spaces :

  • Operating Rooms
  • Emergency Rooms
  • Semiconductor Manufacturing
  • Research labs in colleges and universities

Think you might need more than a phone? Let GAI-Tronics help you build a complete Clean Room Communication System for your clean room facility with the addition of our Clean Room Speakers and other VoIP products. **analog versions also available**

 



Recommended Posts

TEMPERATURE SENSING ACCESS CONTROL FOR ENTRYWAYS

Continue Reading

TOUCHLESS ACCESS CONTROL & SECURITY

Continue Reading
The Power of Voice with Emergency Communications

The Power of Voice with Emergency Communications

Continue Reading