Hubbell Power Systems Blog

How Utilities Use Capacitor Banks for Volt-VAR Optimization

Written by Kevin Corcoran | Jun 18, 2026 3:00:35 PM

Distribution grids are constantly growing in complexity, with rising peak demand, expanding renewable generation, and evolving power-quality requirements. At the same time, utilities are under pressure to deliver stable voltage, high efficiency, and real-time visibility across the feeder.

That is why Volt‑VAR Optimization (VVO) is no longer a forward‑leaning concept; it’s an operational necessity. It transforms power factor correction (PFC) equipment—capacitor banks—into one of the most important tools for maintaining voltage, improving efficiency, and optimizing feeder performance.

Modern capacitor banks do far more than correct power factor. They now sit at the center of the grid regulation, monitoring, and automation strategies that Hubbell Power Systems (HPS) helps utilities implement to run a more resilient, flexible, and efficient distribution system.

Why Capacitor Banks Matter in Volt-VAR Optimization

For decades, utilities installed capacitor banks primarily to fix lagging power factor. Today, that value has expanded dramatically, with capacitor banks playing an important role across a wide range of grid applications.

Stabilizing Feeder Voltage

Capacitor banks support voltage regulation by helping reduce voltage drops along the feeder, especially at its farthest points. Their ability to boost voltage makes them essential to keeping voltage within acceptable ranges under fluctuating load conditions.

Reducing Losses and Improving System Efficiency

By providing reactive power locally for inductive loads, capacitor banks reduce current flow in lines and transformers. This cuts distribution thermal losses and frees up capacity for additional load or DER injection.

Supporting Renewable and DER Integration

As solar and wind installations grow, the grid must manage more variable and less predictable load and voltage swings. Capacitor banks help dampen these fluctuations and maintain power quality, making them critical to higher DER hosting capacity.

Enabling Volt-VAR Optimization

VVO programs rely on coordinated control across voltage regulators, load tap changers (LTCs), and capacitor banks to reduce energy consumption and flatten voltage profiles. Capacitor banks are a critical component of voltage management schemes, and their reactive power is the essential source for managing VARs.

How Utilities Use Capacitor Banks to Regulate and Monitor the Grid

  1. 1. Reactive Power Control That Responds in Real Time

HPS capacitor banks can switch on and off in near real time to respond to changing feeder conditions—shifts in load, DER output, or seasonal patterns. When integrated with a VVO strategy, they coordinate with regulators and other devices to minimize losses and maintain voltage stability.

HPS manufactures a wide variety of transmission, distribution, substation, and telecommunications products that utilities use to add efficiency and resiliency to the grid. Within the Hubbell Utility Solutions (HUS) portfolio, Beckwith Electric’s Volt‑VAR management solutions utilize capacitor banks to serve as the first line of defense for real-time voltage and VAR control.

2. Power Quality and System Health Monitoring

Advanced capacitor bank controllers—whether it’s Beckwith or another option—provide real‑time measurements of voltage, current, power factor, and harmonics.
For example, the Beckwith M‑6283A offers:

    • Three‑phase voltage and current sensing
    • Harmonics monitoring
    • Advanced data logging and oscillography for diagnostics
    • Power quality analytics that support feeder optimization and issue detection

This data integrates directly into SCADA, distribution automation platforms, and other DNP3/Modbus systems and can be used in conjunction with AMI analytics. With this integration, operators can see voltage trends, detect VAR deficiencies, and respond before they impact reliability.

3. Conservation Voltage Reduction (CVR) Enablement

Utilities pursuing CVR depend on the ability to fine‑tune feeder voltage without dropping below minimum voltage levels. Capacitor banks assist by providing a cost-effective means of managing voltage, allowing the system to safely lower voltage while complying with regulatory limits. Beckwith’s VVO/CVR capabilities enable centralized or distributed control between capacitor banks and regulators to maintain reliable service at lower voltage levels.

4. Optimizing Feeder Performance Under High DER Penetration

Circuits with high penetrations of solar power often struggle with mid‑day voltage rise and evening voltage sag. Capacitor banks, combined with intelligent, 3-phase controllers, help balance these swings, improving both hosting capacity and customer voltage stability. Market analyses consistently show DER growth as a major driver of capacitor bank adoption.

The Role of Controllers: Why Standardization Matters

A capacitor bank is only as smart as the controller managing it. And utilities don’t all operate the same way. That’s why standardization and interoperability of capacitor banks and controllers are so essential, and both controller-flexible architectures and Beckwith-based configurations each serve important purposes.

Controller Compatibility Provides Utility Flexibility

Many utilities already standardize controller brands across feeders. There are many reasons that utilities choose to design and source capacitor banks independently from the controller:

  • Maintaining vendor flexibility for engineering and sourcing teams
  • Capacitor banks and controllers often have different lifecycles, depreciation and upgrade schedules
  • Alignment with utility engineering and operations responsibilities for controls versus apparatus

This approach meets utilities where they are by integrating new capacitor banks into existing operational ecosystems without friction.

The Benefits of Single-Source Procurement

Utilities are increasingly seeing valuable benefits for procuring their capacitor banks and controllers together:

  • They get a fully integrated solution
  • Factory tested and packaged solutions are ready for deployment on site, saving time and resources
  • It simplifies maintenance and troubleshooting while reducing finger-pointing

Controllers from Hubbell Power Systems Provide Intelligence for VVO and CVR

When utilities need advanced grid automation, Beckwith controllers from Hubbell unlock deeper capabilities:

Beckwith M‑6283A Highlights

        • Enables (or supports) both ganged and independent phase switching
        • Monitors harmonics, events, and power quality in real time
        • Offers advanced metering and oscillography
        • Supports VVO, CVR, and DER integration
        • Provides cyber-secure communication using DNP3, Modbus, Ethernet, fiber, Blutooth, and more 

Combined with our broader advanced distribution grid solutions, these controls create a coordinated environment where capacitor banks work alongside voltage regulators and LTCs to reduce losses, improve voltage stability, and maintain reliable operation.

Why This Matters

Utilities implementing capacitor banks as part of a VVO strategy gain immediate, measurable benefits:

 ✔ Better Voltage Compliance

Capacitors help maintain voltage across the feeder, even under DER variability.

 ✔ Lower Losses & Cost Savings

Reduced reactive power demand lowers current, losses, and system stress.

✔ Greater DER Hosting Capacity

Improved voltage stability allows more renewable interconnection without infrastructure upgrades.

✔ Enhanced Situational Awareness

With the right controllers and SCADA communications, capacitor banks become real‑time sensors and data sources, not just sources of VARs.

✔ Automated, Optimized Feeder Performance

Capacitor banks form the reactive power backbone of any VVO/CVR system.

Conclusion

Capacitor banks sit at the center of modern VVO solutions. They give utilities the ability to regulate voltage, reduce losses, manage DER variability, and gain real‑time visibility—all while improving power quality and lowering operational costs.

Whether selected and deployed independently of the controller or closely integrated with our advanced VVO-enabled controllers, a well-designed capacitor bank strategy transforms what was once a simple PFC device into a powerful grid‑stabilizing asset.

Explore Hubbell Power Systems’ capacitor bank solutions and power factor correction equipment to learn more.