In today's residential and multifamily construction market, builders face increasing pressure to control costs, accelerate schedules, and build on sites that would have been considered unbuildable just a few decades ago. As housing demand pushes development into areas with difficult soil conditions, many builders are discovering that helical piles provide a cost-effective alternative to traditional foundation systems.
Helical piles are frequently used where challenging soil conditions exist, including:
Versatility and installation efficiency have made helical piles an increasingly attractive solution for both single-family and multifamily projects.
👉 Read about a single-family new construction on a limited access site with unstable soil
For most builders, the primary concern is not the type of foundation being installed - it is total installed cost. While the initial foundation price is important, experienced builders understand that the true cost of a foundation includes:
site preparation
installation time
testing requirements
equipment mobilization
excavation
schedule impacts
potential construction delays
One of the most compelling benefits of helical piles is their ability to reduce total installed foundation costs. Compared to many other foundation types, helical piles typically require less site preparation and smaller installation equipment. Because they are screwed into the ground rather than drilled or driven, installation is often faster and more predictable.
Helical piles can generally support design loads immediately after installation, subject to the project engineer's requirements and any specified verification or load testing. Traditional concrete foundations often require curing time before structural loads can be applied and may involve quality-control procedures such as slump and cylinder testing. By avoiding concrete curing delays, helical piles can allow framing and other structural work to begin sooner. For production builders, apartment developers, and general contractors, days removed from the schedule can contribute to lower carrying costs and earlier project completion.
Since helical pile installation generally requires little or no excavation, and because soil is not removed from the ground, there are typically no spoils to haul away or dispose of. This is particularly beneficial on tight urban sites.
👉 Read a case study of a multi-family home constructed on weathered rock
For builders working in developed neighborhoods or on constrained lots, helical piles offer another significant benefit: installation in limited-access areas. Unlike many deep foundation systems that require large drilling rigs or pile-driving equipment, helical piles are often installed using compact equipment, such as a skid steer loader or mini-excavator, that can operate in restricted spaces. This makes them particularly attractive for infill construction, townhome developments, custom homes with limited setbacks, and multifamily projects where property lines, existing structures, or overhead obstructions limit access. Because of the installation method, vibration and noise will not affect neighboring people or structures.
👉 Read a case study where the building was occupied during foundation construction
The ability to build in difficult ground conditions is another reason builders choose helical piles. Many regions throughout North America contain soils that create challenges for traditional shallow foundations:
Helical piles can often be advanced through these problematic soils to reach more suitable bearing strata, improving foundation performance and reducing settlement risk.
👉 Read about a beach front new home construction in Hawaii
Builders are also increasingly focused on sustainability and environmental stewardship. Helical piles are often viewed as an environmentally friendly foundation alternative because they require minimal excavation, generate little waste, and can often be removed or repurposed if site conditions change. Environmentally sensitive properties, and sites with contaminated soils where soil handling or disposal is a concern can often be built on due to the lack of soil disturbance caused by helical piles. Reduced disturbance also minimizes disruption to neighboring structures and decreases the environmental footprint of construction activities.
👉 Read about a brownfield site installation in South Carolina
Their ability to be installed during a wide range of weather conditions, including frozen ground, further contributes to construction flexibility and reduced schedule risk. In colder climates, helical piles are commonly used in frost-susceptible areas and have demonstrated excellent performance in frozen ground and permafrost applications.
👉 Read about a frozen ground installation in Alaska
Beyond building foundations, builders and developers are finding additional uses for helical pile technology. Helical pile foundations can support Level 2 electric vehicle charging stations, parking lot lighting, pedestrian lighting, signage, solar structures, and other site improvements. These applications allow developers to use a single foundation technology across multiple project components while maintaining the benefits of rapid installation and immediate loading.
As residential and multifamily development continues to move onto more challenging sites, builders are increasingly evaluating foundation systems based on total installed cost rather than simply material cost. Helical piles offer a compelling combination of speed, efficiency, minimal site disruption, and reliable performance in difficult ground conditions. For builders seeking to reduce risk, accelerate schedules, and improve overall project economics, helical piles have become a foundation solution worth serious consideration.
Contact your local Chance distributor to see if helical piles are right for your next project.