What is Wi-Fi 7? A Guide to Future-Proof Your Network

Explore the key benefits and challenges of Wi-Fi 7 and gain expert recommendations on preparing your network to leverage this cutting-edge technology

Preparing for Wi-Fi 7
What is Wi-Fi 7? A Guide to Future-Proof Your Network
5:06

Wi-Fi 7 and Its Implications

The release of Wi-Fi 7 is framed as one of the biggest networking revolutions in over 20 years. Wi-Fi 7, known technically as 802.11be, is set to deliver substantial enhancements over its predecessors, Wi-Fi 6 and Wi-Fi 6E. This latest standard is designed to significantly improve throughput, reduce latency, and boost efficiency, especially in densely populated areas.  

Wi-Fi 7 introduces multi-link operation, broader channel widths, and advanced modulation techniques to facilitate higher data transmission. Designed to overcome challenges previous Wi-Fi standards face, Wi-Fi 7 excels in streaming multiple 4K/8K video feeds, supporting AR/VR applications, and enabling ultra-low-latency gaming. 

Technical Advancements of Wi-Fi 7  

Wi-Fi 7 is more than just an upgrade; its technical improvements represent a significant advancement in digital connectivity. With these capabilities, Wi-Fi 7 is ideally positioned to future-proof IoT infrastructures and significantly enhance both scheduling efficiency and client management. 

Key Features: 

  • Multi-Link Operation (MLO): Devices can use multiple radios or channels simultaneously to increase bandwidth and network resilience. 
  • 320 MHz Channel Widths: This wider spectrum allows for more data throughput, supporting more simultaneous data transmissions. 
  • 4096-QAM (Quadrature Amplitude Modulation): A more complex modulation scheme to carry more bits per symbol, optimizing performance in conditions with very high signal-to-noise ratios.  

What to Expect with Wi-Fi 7 Adoption 

As Wi-Fi 7 continues to roll out, early adopters such as high-end routers and enterprise-grade Wi-Fi equipment are likely to be the first to embrace this new technology. The transition to Wi-Fi 7 won't happen overnight. It will be a gradual process where networks will support both Wi-Fi 6 and Wi-Fi 7 devices, allowing systems to adjust seamlessly without disrupting existing setups. Ultimately, the full benefits of Wi-Fi 7 will be realized with its widespread adoption across various devices and environments.  

Key Challenges in Wi-Fi 7 Implementation:  

  • Spectrum availability: The real-world performance depends heavily on having clean spectrum (i.e. less interference) especially in the 6 GHz band. 
  • Device support: Both clients (phones, laptops, etc.) and access points must support the new standard for the gains to be realized. A transition period will persist. 
  • Backhaul constraints: Even if Wi-Fi 7 radios can push faster data, the network’s wired backbone (or upstream link) may become the bottleneck. 
  • Cost & complexity: Implementing support for multi-link and wide channels can increase hardware cost, power consumption, and design complexity. 
  • Regional differences: Different countries have different regulations about which bands (especially in 6 GHz) are usable for unlicensed Wi-Fi, which may slow adoption in some regions. 

Essential Steps to Prepare your Network for WiFi-7  

The introduction of Wi-Fi 7 brings significant implications for data communication networks. For organizations considering an upgrade, here are some essential steps to prepare: 

  1. 1. Check whether your devices (clients & APs) are compatible with Wi-Fi 7. 

  2. 2. Ensure your entire network infrastructure can handle the increased demand. Upgrading routers prematurely might not yield big gains unless the rest of your network (and internet link) can keep up.   

  3. 3. Assess Power over Ethernet (PoE) strain. Wi-Fi 7 access points (APs) may require more power (60-71.3W per port) to operate at their full potential, potentially exceeding the capacity of existing PoE switches and necessitating network upgrades. 

  4. 4. Watch for crucial firmware and hardware updates from vendors that unlock Wi-Fi 7 features.

  5. 5. In some environments, optimal performance will require careful channel planning and interference mitigation.  

Explore Wi-Fi 7 Accessories from Hubbell 

To fully harness the capabilities of Wi-Fi 7, consider upgrading to the following Hubbell datacom accessories designed to support high-performance Wi-Fi 7 deployments:

Tri-band Antennas

Acceltex and Ventev are ready with Tri-band Antennas compatible with all Wi-Fi 7 AP models that use external antennas, ensuring optimal signal quality and coverage.

Cat6a Ethernet Cable

Hubbell Premise Wiring Copper Cabling supports the higher speeds and performance needed by Wi-Fi 7 access points (APs).

Ready to Upgrade? Reach out to a Network Expert  

Don't navigate the complexities of upgrading to Wi-Fi 7 alone. Connect with our team of industry experts and benefit from tailored product recommendations and strategic network design insights. The future of Wi-Fi is here—make sure your network is ready.

Contact us for expert guidance in transitioning your network to Wi-Fi 7.



Recommended Posts

resolve-tx-power-mismatch

WLPC Prague 2024: How higher gain antennas resolve Tx power mismatch

Continue Reading

AccelTex Solutions Releases new video guide for the Staggered AP and Antenna Mount

Continue Reading

Warehouse Wi-Fi Design

Continue Reading