Latest news

Austdac Pullkey - Aluminium Crimp Safety Notices
As previously notified Austdac is voluntarily notifying customers that, due to an error by our production partner, certain Austdac branded Pullkey products manufactured between January 2020 and March...
Continue reading
AC25W PRODUCT OBSOLESCENCE NOTIFICATION
The AC25W power supply certified under IECEx TSA 07.0031X is obsolete and will no longer be manufactured.
Continue reading
Austdac UPS (UPS12NMH288-1000)
The Austdac UPS (Uninterruptible Power Supply) uses Ni-MH (Nickel metal hydride) batteries. The Austdac UPS design minimises the stress on the Ni-MH batteries by ensuring the batteries are charged at...
Continue reading
Austdac UPS (UPS12NMH288-1000-A)
The Austdac UPS (Uninterruptible Power Supply) is available in two versions, A and B. The UPS12NMH288-1000-A (A version) has an integrated 10m Type 2S mains cable. The user usually cuts this cable to...
Continue reading
TROLEX TX6383 INCORRECT CERTIFICATE OF CONFORMITY NUMBER
It has been found that a small number of TX6383 have been sent to customers with an incorrect certificate of conformity number on their label. The incorrect certificate of conformity number issued...
Continue reading
ALR3 New Product ALR2 Obsolescence Notification
Austdac has released the Alarm Latch Relay 3 (ALR3) which is certified under IECEx certificate number IECEx ExTC 19.0017X.
Continue reading
TX6363, TX6373 and TX6383 Mixing ANZEx and AUSEx Certificates Advisory
This advisory is applicable to the Trolex Gas Detector, TX6363, TX6373 and TX6383, distributed by Austdac Pty Ltd. The following Trolex Gas Detectors have been sold with the following certificates of...
Continue reading
CSE SR50 and SR100A Self Rescuers Advisory Follow Up
During 2016 and 2017 Austdac inspected SR50 and SR100A manufactured in 2011 and earlier as part of an Austdac advisory dated the 26th of April 2016. As a result of this inspection a total of 4735...
Continue reading
AD101 and AD102 Mine Phone End of Life Advisory Use of A103 on ST/1 System Advisory
The IS Telephones AD101 and AD102 have been in service for 38 years and from March 2017 Austdac will no longer be able to repair these due to the parts no longer being available. The Austdac...
Continue reading
CSE SR50 and SR100A Self Rescuers Advisory
In 2016 Austdac began a program to perform an internal inspection on the SR50 and SRIOOA Self Rescuers due to possible mishandling of the units. During these inspections it was found in a number of...
Continue reading