Aclara Technologies Blog

Choosing the Right Communications Network for Modern Utility Operations

Written by Aclara | Aug 13, 2026, 2:57:34 PM

As utilities modernize grid operations, communications networks are playing a larger role in moving data between field devices, meters, and control systems.

Advanced metering infrastructure (AMI), grid monitoring, and other digital grid applications depend on reliable connectivity to deliver timely information and support operational decision-making. As these demands grow, utilities are evaluating whether their communications infrastructure can support both current needs and future requirements.

That evaluation is bringing renewed attention to Aclara’s 450 MHz RF point-to-multipoint network approach, which is engineered to deliver dependable, two-way communications to more than 99% of endpoints, even during outage conditions.

How a 450 MHz RF Network Improves Utility Communications

Today’s grid is more connected and data-driven than ever before. Utilities must communicate with meters and devices in challenging locations, including inside buildings, behind concrete walls, or underground, while ensuring reliable and secure data delivery.

Because 450 MHz operates at a lower frequency, it provides stronger propagation characteristics. The signal travels farther and penetrates dense materials like concrete and steel more effectively, improving communication in basements, vaults, and urban environments where higher-frequency signals often struggle.

Combined with Aclara’s network redundancy design, where each meter communicates directly with two or more data collector units (DCUs), utilities benefit from multiple communication paths that improve both reliability and data resilience.

For utilities leveraging an Aclara 450 MHz network, this results in more consistent connectivity and stronger overall system performance.

Expanding Coverage Without Adding Complexity

450 MHz also enables broader geographic reach. Its longer wavelength allows signals to travel greater distances, reducing the infrastructure required to cover a service area.

Aclara’s point-to-multipoint architecture helps utilities simplify network design across diverse terrains while maintaining strong performance.

In fact, improved signal propagation means fewer DCUs are required, enabling faster deployment timelines and lowering upfront capital investment.

A More Reliable Spectrum Environment

The unlicensed 900 MHz band is widely used across industries, which can introduce interference and variability. In contrast, 450 MHz operates within a licensed spectrum, creating a more controlled and predictable communications environment.

The use of licensed 450–470 MHz spectrum reduces signal path loss, providing a private network for the utility that supports consistent, reliable performance across urban, suburban, and rural environments. This stability helps ensure critical data is delivered without disruption.

Why Utilities Choose Private Utility Communications Networks

With a private network, utilities maintain full ownership and control of their communications infrastructure rather than relying on shared or public systems.

Operating on utility-controlled, FCC-issued licensed channels, the network provides enhanced security through NIST-compliant authenticated messaging and AES-256 encryption, ensuring high data integrity across the system.

This control supports evolving grid demands, including distributed energy resources and advanced monitoring.

AMI Meters Optimized for 450 MHz Networks

Aclara’s portfolio of meters, including the I-210+, I-210+c residential meter, and the kV2c Gen5 commercial meters, is engineered to deliver reliable AMI communication across challenging conditions, ensuring consistent data delivery from the field.

Because the network supports multiple applications on a common infrastructure, including electric, gas, and water AMI, demand response, distribution automation, and grid sensing, these meters become part of a broader, unified system managed through the AclaraONE® software headend.

Building a Future-Ready Utility Communications Network

Utilities are planning to increase data demands and expand grid complexity requiring their communications network to scale accordingly.

With up to 35% lower operational and capital costs compared to many RF network alternatives, Aclara’s 450 MHz point-to-multipoint approach delivers a compelling total cost of ownership advantage across the full system lifecycle. This network solution offers a clear path forward, providing the coverage, reliability, and control utilities need to move confidently into the future.

In an increasingly connected world, the right foundation makes all the difference.

Explore Aclara's Utility Communications Networks