CHALLENGE: Client needed a custom Wi-Fi set-up that was also aesthetically pleasing In a high-density environment (Arena) A need to develop custom-shaped enclosures with custom backplates and angled mounts inside SOLUTION: Developed custom enclosures Backplates and mounts inside of the enclosure can be easily adjusted Enclosures are colored or skinned to match their environment… Read More
CHALLENGE:
Client needed a custom Wi-Fi set-up that was also aesthetically pleasing
In a high-density environment (Arena)
A need to develop custom-shaped enclosures with custom backplates and angled mounts inside
SOLUTION:
Developed custom enclosures
Backplates and mounts inside of the enclosure can be easily adjusted
Enclosures are colored or skinned to match their environment
Custom handrail antennas to focus RF coverage down both sides of aisles